AXIS#.BODE.INJECTPOINT

Description

AXIS#.BODE.INJECTPOINT sets whether the excitation uses current or velocity excitation type.

AXIS#.BODE.INJECTPOINT

Description

0

None

1

Current

2

Velocity

Example

Set AXIS1.BODE.INJECTPOINT to current:

-->AXIS1.BODE.INJECTPOINT 1

Get AXIS1.BODE.INJECTPOINT (already set to current):

-->AXIS1.BODE.INJECTPOINT 1

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 2

Default Value

0

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.BODE.INJECTPOINT 0x5001 0x1 USINT - - RW False
AXIS2.BODE.INJECTPOINT 0x5101 0x1 USINT - - RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen